Everything

2.9 Start Program Analyzer Tool [RI850V4 V1.xx.xx][RI78V4 V1.xx.xx]

From [View] menu, select [Realtime OS] >> [Program Analyzer], program analyzer is started.
From [View] menu, select [Realtime OS] >> [Program Analyzer]. The program analyzer is started.
Figure 2-8. [Program Analyzer] Item
Figure 2-9. Program Analyzer Window
Remarks 1. When program analyzer has started, it isn't possible to start more program analyzer.
2. See "RI850V4/RI78V4 Analysis" for details.