Everything

2.3 Create a Project for RI Series

The creation of a project for RI series is performed with the Create Project dialog box (See the CS+ Start "2.6.2 Create a new project").
From the [Project] menu, select [Create New Project...], the following dialog box will open.
Figure 2-3. Create Project Dialog Box
Select the item below on [Kind of project].
- Application(RI series name, Build tool name)
Select this to generate a project for RI series.