12-bit A/D converter
Below is a list of API functions output by the Code Generator for 12-bit A/D converter use.
Table 3.49 API Functions: [12-bit A/D Converter]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the 12-bit A/D converter.  | |
| 
       Performs user-defined initialization relating to the 12-bit A/D converter.  | |
| 
       Performs processing in response to the A/D conversion end interrupt INTAD.  | |
| 
       Starts A/D conversion.  | |
| 
       Ends A/D conversion.  | |
| 
       Reads the results of A/D conversion (12 bits).  | |
| 
       Configures the analog voltage input pin for A/D conversion.  | |
| 
       Enables 12-bit A/D converter temperature sensor output circuit.  | |
| 
       Disables12-bit A/D converter temperature sensor output circuit.  | |
| 
       Enables 12-bit A/D converter reference voltage circuit.  | |
| 
       Disables12-bit A/D converter reference voltage circuit.  | |
| 
       Halts the clock supplied to the 12-bit A/D converter.  |