Timer array unit
Below is a list of API functions output by the Code Generator for timer array unit use.
Table 3.5 API Functions: [Timer Array Unit]
|
API Function Name |
Function |
|
Performs initialization necessary to control the timer array unit. | |
|
Performs user-defined initialization relating to the timer array unit. | |
|
Performs processing in response to the timer interrupt INTTMmn. | |
|
Performs processing in response to the timer interrupt INTTMmnH. | |
|
Starts the count for channel n. | |
|
Starts the count (higher 8-bit) for channel n. | |
|
Starts the count (lower 8-bit) for channel n. | |
|
Ends the count for channel n. | |
|
Ends the count (higher 8-bit) for channel n. | |
|
Ends the count (lower 8-bit) for channel n. | |
|
Reset the timer array unit. | |
|
Halts the clock supplied to the timer array unit. | |
|
Captures the high/low-level width measured between pulses of the signal (pulses) input to the TImn pin. | |
|
Generates the trigger (software trigger) for one-shot pulse output. |