Serial interface IICA
Below is a list of API functions output by the Code Generator for serial interface IICA use.
Table 3.34 API Functions: [Serial Interface IICA]
|
API Function Name |
Function |
|
Performs initialization necessary to control the serial interface IICA. | |
|
Performs user-defined initialization related to the serial interface IICA. | |
|
Performs processing in response to the IICA communication end interrupt INTIICAn. | |
|
Generates stop conditions. | |
|
Ends IICA communication. | |
|
Reset the serial interface IICA. | |
|
Halts the clock supplied to the serial interface IICA. | |
|
Starts IICA master transmission. | |
|
Starts IICA master reception. | |
|
Performs processing in response to the IICA master transmission end interrupt INTIICAn. | |
|
Performs processing in response to the IICA master reception end interrupt INTIICAn. | |
|
Performs processing in response to detection of IICA master communication error. | |
|
Starts IICA slave transmission. | |
|
Starts IICA slave reception. | |
|
Performs processing in response to the IICA slave transmission end interrupt INTIICAn. | |
|
Performs processing in response to the IICA slave reception end interrupt INTIICAn. | |
|
Performs processing in response to detection of IICA slave communication error. | |
|
Performs processing in response to detection of stop condition. | |
|
Enables operation of the address match wakeup function in STOP mode. | |
|
Disables operation of the address match wakeup function in STOP mode. | |
|
Enables operation of the address match wakeup function in STOP mode. | |
|
Disables operation of the address match wakeup function in STOP mode. |