A/D converter
Below is a list of API functions output by the Code Generator for A/D converter use.
Table 3.22 API Functions: [A/D Converter]
|
API Function Name |
Function |
|
Performs initialization necessary to control the A/D converter. | |
|
Performs user-defined initialization relating to the A/D converter. | |
|
Performs processing in response to the A/D conversion end interrupt INTAD. | |
|
Enables operation of voltage converter. | |
|
Disables operation of voltage converter. | |
|
Starts A/D conversion. | |
|
Ends A/D conversion. | |
|
Reset A/D conversion. | |
|
Halts the clock supplied to the A/D converter. | |
|
Configures the analog voltage input pin for A/D conversion. | |
|
Enables the switch from STOP mode to SNOOZE mode. | |
|
Disables the switch from STOP mode to SNOOZE mode. | |
|
Sets the operation mode of A/D converter. | |
|
Reads the results of A/D conversion (10 bits). | |
|
Reads the results of A/D conversion (10 bits). |