This dialog box is used to set an offset value of the start address in the address area on the Memory panel.
![](Debug_RL78_E-749.gif)
This section describes the following.
On the Memory panel, select [View] >> [Address Offset Value Settings...] from the context menu. |
Directly enter a hexadecimal value as an offset value for the address display.
The settable range depends on the number of bytes of the memory currently being displayed in a line on the Memory panel, as follows:
When "Set value of [Size Notation]" is 1 byte and "The number of view columns" is 16 columns: |