Everything

del_alm

Outline
Delete alarm handler.
C format
 ER      del_alm (ID almid);
Parameter(s)
I/O
Parameter
Description
I
 ID      almid;
ID number of the alarm handler.

Explanation
This service call can be called from tasks that belong to Trusted Domain.
This service call deletes the alarm handler indicated by almid.
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_ID
-18
Invalid ID number.
- almid < 0
- almid > VTMAX_ALH
E_CTX
-25
Context error.
- This service call was issued in the CPU locked state.
- This service call was issued from non-task.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
E_MACV
-26
Memory access violation.
- Stack pointer points out of user stack for invoking task.
E_OACV
-27
Object access violation.
- The invoking task does not belong to trusted domain.
E_NOEXS
-42
Non-existent object.
- The alarm handler specified by almid does not exist.