stp_alm
istp_alm
ER stp_alm (ID almid);
ER istp_alm (ID almid);
This service call moves the alarm handler specified by parameter almid from the operational state (STA state) to non-operational state (STP state).
As a result, the target alarm handler is excluded from activation targets of the RI600PX until issuance of sta_alm or ista_alm.
Note This service call does not perform queuing of stop requests. If the target alarm handler has been moved to the non-operational state (STP state), therefore, no processing is performed but it is not handled as an error.