stp_cyc
istp_cyc
ER stp_cyc (ID cycid);
ER istp_cyc (ID cycid);
This service call moves the cyclic handler specified by parameter cycid from the operational state (STA state) to non-operational state (STP state).
As a result, the target cyclic handler is excluded from activation targets of the RI600PX until issuance of sta_cyc or ista_cyc.
Note This service call does not perform queuing of stop requests. If the target cyclic handler has been moved to the non-operational state (STP state), therefore, no processing is performed but it is not handled as an error.