CHAPTER 5 SYNCHRONIZATION AND COMMUNICATION FUNCTIONS
The synchronization and communication functions of the RI600V4 consist of Semaphores, Eventflags, Data Queues, and Mailboxes that are provided as means for realizing exclusive control, queuing, and communication among tasks.
In the RI600V4, non-negative number counting semaphores are provided as a means (exclusive control function) for preventing contention for limited resources (hardware devices, library function, etc.) arising from the required conditions of simultaneously running tasks.
Semaphores therefore cannot be created dynamically using a method such as issuing a service call from a processing program.
Static semaphore creation means defining of semaphores using static API "semaphore[]" in the system configuration file.
For details about the static API "semaphore[]", refer to "19.8 Semaphore Information (semaphore[])".
A resource is acquired (waiting forever, polling, or with time-out) by issuing the following service call from the processing program.
- wai_sem (Wait)
This service call acquires a resource from the semaphore specified by parameter semid (subtracts 1 from the semaphore counter).
When no resources are acquired from the target semaphore when this service call is issued (no available resources exist), this service call does not acquire resources but queues the invoking task to the target semaphore wait queue and moves it from the RUNNING state to the WAITING state (resource acquisition wait state).
The WAITING state for a semaphore resource is cancelled in the following cases.
This service call acquires a resource from the semaphore specified by parameter semid (subtracts 1 from the semaphore counter).
When no resources are acquired from the target semaphore when this service call is issued (no available resources exist), this service call does not acquire resources but queues the invoking task to the target semaphore wait queue and moves it from the RUNNING state to the WAITING state (resource acquisition wait state).
The WAITING state for a semaphore resource is cancelled in the following cases.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600*/ void task (VP_INT exinf) { ER ercd; /*Declares variable*/ ID semid = 1; /*Declares and initializes variable*/ /* ......... */ ercd = wai_sem (semid ); /*Acquire semaphore resource*/ if (ercd == E_OK) { /* ......... */ /*Normal termination processing*/ sig_sem ( semid ); /*Release semaphore resource*/ } else if (ercd == E_RLWAI) { /* ......... */ /*Forced termination processing*/ } /* ......... */ } |
Note Invoking tasks are queued to the target semaphore wait queue in the order defined during configuration (FIFO order or current priority order).
- pol_sem, ipol_sem (Polling)
These service calls acquire a resource from the semaphore specified by parameter semid (subtracts 1 from the semaphore counter).
If a resource could not be acquired from the target semaphore (semaphore counter is set to 0) when these service calls are issued, the counter manipulation processing is not performed but E_TMOUT is returned.
The following describes an example for coding these service calls.
These service calls acquire a resource from the semaphore specified by parameter semid (subtracts 1 from the semaphore counter).
If a resource could not be acquired from the target semaphore (semaphore counter is set to 0) when these service calls are issued, the counter manipulation processing is not performed but E_TMOUT is returned.
The following describes an example for coding these service calls.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600*/ void task (VP_INT exinf) { ER ercd; /*Declares variable*/ ID semid = 1; /*Declares and initializes variable*/ /* ......... */ ercd = pol_sem (semid); /*Acquire semaphore resource*/ if (ercd == E_OK) { /* ......... */ /*Polling success processing*/ sig_sem ( semid ); /*Release semaphore resource*/ } else if (ercd == E_TMOUT) { /* ......... */ /*Polling failure processing*/ } /* ......... */ } |
- twai_sem (Wait with time-out)
This service call acquires a resource from the semaphore specified by parameter semid (subtracts 1 from the semaphore counter).
If no resources are acquired from the target semaphore when service call is issued this (no available resources exist), this service call does not acquire resources but queues the invoking task to the target semaphore wait queue and moves it from the RUNNING state to the WAITING state with time-out (resource acquisition wait state).
The WAITING state for a semaphore resource is cancelled in the following cases.
This service call acquires a resource from the semaphore specified by parameter semid (subtracts 1 from the semaphore counter).
If no resources are acquired from the target semaphore when service call is issued this (no available resources exist), this service call does not acquire resources but queues the invoking task to the target semaphore wait queue and moves it from the RUNNING state to the WAITING state with time-out (resource acquisition wait state).
The WAITING state for a semaphore resource is cancelled in the following cases.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600*/ void task (VP_INT exinf) { ER ercd; /*Declares variable*/ ID semid = 1; /*Declares and initializes variable*/ TMO tmout = 3600; /*Declares and initializes variable*/ /* ......... */ ercd = twai_sem (semid, tmout); /*Acquire semaphore resource*/ if (ercd == E_OK) { /* ......... */ /*Normal termination processing*/ sig_sem ( semid ); /*Release semaphore resource*/ } else if (ercd == E_RLWAI) { /* ......... */ /*Forced termination processing*/ } else if (ercd == E_TMOUT) { /* ......... */ /*Time-out processing*/ } /* ......... */ } |
Note 1 Invoking tasks are queued to the target semaphore wait queue in the order defined during configuration (FIFO order or current priority order).
Note 2 TMO_FEVR is specified for wait time tmout, processing equivalent to wai_sem will be executed. When TMO_POL is specified, processing equivalent to pol_sem will be executed.
- sig_sem, isig_sem
These service calls releases the resource to the semaphore specified by parameter semid (adds 1 to the semaphore counter).
If a task is queued in the wait queue of the target semaphore when this service call is issued, the counter manipulation processing is not performed but the resource is passed to the relevant task (first task of wait queue).
As a result, the relevant task is unlinked from the wait queue and is moved from the WAITING state (WAITING state for a semaphore resource) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
The following describes an example for coding these service calls.
These service calls releases the resource to the semaphore specified by parameter semid (adds 1 to the semaphore counter).
If a task is queued in the wait queue of the target semaphore when this service call is issued, the counter manipulation processing is not performed but the resource is passed to the relevant task (first task of wait queue).
As a result, the relevant task is unlinked from the wait queue and is moved from the WAITING state (WAITING state for a semaphore resource) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
The following describes an example for coding these service calls.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600*/ void task (VP_INT exinf) { ER ercd; /*Declares variable*/ ID semid = 1; /*Declares and initializes variable*/ /* ......... */ ercd = wai_sem (semid ); /*Acquire semaphore resource*/ if (ercd == E_OK) { /* ......... */ /*Normal termination processing*/ sig_sem ( semid ); /*Release semaphore resource*/ } else if (ercd == E_RLWAI) { /* ......... */ /*Forced termination processing*/ } /* ......... */ } |
Note With the RI600V4, the maximum possible number of semaphore resources (maximum resource count) is defined during configuration. If the number of resources exceeds the specified maximum resource count, this service call therefore does not release the acquired resources (addition to the semaphore counter value) but returns E_QOVR.
- ref_sem, iref_sem
Stores semaphore state packet (ID number of the task at the head of the wait queue, current resource count, etc.) of the semaphore specified by parameter semid in the area specified by parameter pk_rsem.
The following describes an example for coding these service calls.
Stores semaphore state packet (ID number of the task at the head of the wait queue, current resource count, etc.) of the semaphore specified by parameter semid in the area specified by parameter pk_rsem.
The following describes an example for coding these service calls.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600*/ void task (VP_INT exinf) { ID semid = 1; /*Declares and initializes variable*/ T_RSEM pk_rsem; /*Declares variable*/ ID wtskid; /*Declares variable*/ UINT semcnt; /*Declares variable*/ /* ......... */ ref_sem ( semid, &pk_rsem ); /*Reference semaphore state*/ wtskid = pk_rsem.wtskid; /*Reference ID number of the task at the */ /*head of the wait queue*/ semcnt = pk_rsem.semcnt; /*Reference current resource count*/ /* ......... */ } |