APPENDIX C DSP FUNCTION
When a MCU which support the DSP function is used, it is necessary to note the treatment of the ACC register (accumulator). Concretely, please note it as follows when you use the following DSP instructions which update ACC register.
- RXv2 architecture instructions
EMACA, EMSBA, EMULA, MACLH, MSBHI, MSBLH, MSBLO, MULLH, MVTACGU, RACL,RDACL, RDACW
EMACA, EMSBA, EMULA, MACLH, MSBHI, MSBLH, MSBLO, MULLH, MVTACGU, RACL,RDACL, RDACW
Note also that if the "-chkdsp" option is specified in the assembler, the DSP function instructions written in a program are detected as warning.
Make settings that include "ACC" for Task context register (context) in System Information (system). As a result, the ACC register is managed independently in each task.
If the application contains any tasks or interrupt handlers that use the above-mentioned DSP instructions, it is necessary that all of the interrupt handlers guarantee the ACC register. There are the following two method.
2 ) Specify "ACC" for "pragma_switch" in all interrupt handler definition (Relocatable Vector Information (interrupt_vector[]) and Fixed Vector/Exception Vector Information (interrupt_fvector[])).