< Compile Options / Optimize Options >
[Format]
[Description]
- | When the noinline option is specified, automatic inline expansion is not performed. |
[Remarks]
- | Expansion is attempted for the functions with #pragma inline specified regardless of the specification of this option. The inline function specifier (C99) is effective only when this option is invalid. |