Everything

-whole_program


< Compile Options / Optimize Options >

[Format]

-whole_program

[Description]

-

This option makes the compiler perform optimization on the assumption that all source files have been input.

[Remarks]

-

When this option is specified, do not include C++ language source files among the input files.

-

When this option is specified, do not specify -lang=cpp or -lang=ecpp.

-

Specifying this option also makes the ip_optimize option effective, and if multiple source files are input, the merge_files option is also effective.

-

When this option is specified, compilation is on the assumption that the conditions listed below are satisfied. Correct operation is not guaranteed otherwise.

-

Values and addresses of extern variables defined in the target source files will not be modified or referred to by other files.

-

Functions within the target source file will not be called from within other files, although functions in other files can be called from within the target source files.

[Example]

[wp.c]
extern void g(void);
int func(void)
{
    static int a = 0;
    a++;      // (1) Write a value to a.
    g();      // (2) Call g().
    return a; // (3) Call a.
}
 
[Without whole_program]
The compiler assumes that (2) will change the value of a since function g() may call function func(), and generates a code to read the value of a in (3).
_func:
        PUSH.L R6
        MOV.L  #__$a$1,R6
        MOV.L  [R6],R14
        ADD    #1,R14
        MOV.L  R14,[R6]     ; (1)
        BSR    _g           ; (2)
        MOV.L  [R6],R1      ; (3)
        RTSD   #4,R6-R6
 
[With whole_program]
The compiler assumes that function g() will not call function func() and thus (2) will not change the value of a. As a result, the compiler does not read the value of a in (3) and instead generates a code to use the value written to a in (1).
_func:
        PUSH.L R6
        MOV.L  #__$a$1,R14
        MOV.L  [R14],R6
        ADD    #1,R6
        MOV.L  R6,[R14]     ; (1)
        BSR    _g           ; (2)
        MOV.L  R6,R1        ; (3)
        RTSD   #4,R6-R6