Everything

-tfu_version [V3.05.00 or later]


< Compile Options / Optimize Options >

[Format]

-tfu_version={v1|v2}

 

-

Interpretation when omitted

If the -tfu option is not specified, nothing is assumed to be specified. If the -tfu option is specified, v1 is assumed to be specified.

[Description]

-

Selects the version of the trigonometric function unit. When v1 is specified, TFUv1 is selected. When v2 is specified, TFUv2 is selected.

-

If this option is specified with the -tfu option not specified, an error (E0511152) occurs.