Everything

-isa


< Compile Options / Microcontroller Options >

[Format]

-isa={ rxv1 | rxv2 | rxv3 }

 

-

[Default]

The default for this option is determined based on the environment variable ISA_RX.

[Description]

-

This option specifies an instruction-set architecture for use in generating object files.

[Remarks]

-

When neither the -nofpu nor -fpu option has been selected, specifying this option automatically selects the -fpu option.

-

Omitting this option when neither the -cpu option nor one of the environment variables (CPU_RX or ISA_RX) is specified will lead to an error.

-

When the -cpu option and this option are specified simultaneously, an error will occur.