Everything

-branch


< Compile Options / Microcontroller Options >

[Format]

-branch = { 16 | 24 | 32 }

 

-

[Default]

The default for this option is branch=24.

[Description]

-

This option specifies the branch width.

-

When branch=16 is specified, the program is compiled with a branch width within 16 bits.

-

When branch=24 is specified, the program is compiled with a branch width within 24 bits.

-

When branch=32 is specified, the branch width is not specified.