Everything

-patch


< Compile Options / Microcontroller Options >

[Format]

-patch = { rx610 }

[Description]

-

This option is used to avoid a problem specific to the CPU type.

-

When -patch=rx610 is specified, the MVTIPL instruction which causes a problem in the RX610 Group is not used in the generated code. Unless -patch=rx610 is specified, the code generated in response to the call by the intrinsic function set_ipl will contain the MVTIPL instruction.