Everything

-endian


< Compile Options / Microcontroller Options >

[Format]

-endian={ big  |  little }

 

-

[Default]

The default for this option is endian=little.

[Description]

-

When endian=big is specified, data bytes are arranged in big endian.

-

When endian=little is specified, data bytes are arranged in little endian.

-

The mode for arranging data bytes can also be specified by the #pragma endian directive. If both this option and a #pragma directive are specified, the #pragma specification takes priority.