Everything

[Mutex] tab

This tab displays the mutex information (e.g. Mutex Name and ID) of the RI600PX.
Figure A-17. [Mutex] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
(a) First layer
This layer displays the mutex information (e.g. Mutex Name and ID) of the RI600PX.
This layer consists of the following items.
Mutex Name
An icon indicating the current status of the mutex and the name of the mutex are shown in the following format.
Icon Name
There are waiting tasks.
There are no waiting tasks. (The task locking the mutex)
There are no waiting tasks.
Non-existent mutex
ID
The ID of the mutex is shown.
Queue Status
The current status of the mutex is shown.
Waiting Tasks
There are waiting tasks.
Empty
There are no waiting tasks.
Locking Task ID
The ID of the locking task is shown.
Attribute
The attributes of the mutex is shown.
TA_CEILING
Priority ceiling protocol
Ceiling Priority
The ceiling priority of the mutex is shown.

(b) Second layer
The waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the mutex's wait queue.
See the [Task] tab for details about waiting task information.
Figure A-18. [Mutex] Tab (Waiting Task Information)
[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Mutex Name, ID, Queue Status, Locking Task ID, Attribute, Ceiling Priority
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
ID, Locking Task ID, Ceiling Priority
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Reset Display Item
Resets the item displayed to initial state.