Everything

[Ready Queue] tab

This tab displays the ready queue information (e.g. Priority and Task Num) of the RI600PX.
Figure A-27. [Ready Queue] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
(a) First layer
This layer displays the ready queue information (e.g. Priority and Task Num) of the RI600PX.
This layer consists of the following items.
Priority
An icon indicating the current status of the ready queue and the task priority are shown in the following format.
Icon Task priority
There are queued tasks.
There are no queued tasks.
Number of Tasks
The total number of queued tasks (tasks with of READY state or RUNNING state) is shown.

(b) Second layer
The executing task information (e.g. Task Name and ID) only appears if there are tasks queued in the ready queue.
See the [Task] tab for details about executing task information.
Figure A-28. [Ready Queue] Tab (Executing Task Information)
[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Priority, Number of Tasks
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
Priority, Number of Tasks
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Reset Display Item
Resets the item displayed to initial state.