|
|
An icon indicating the current status of the cyclic handler and the name of the cyclic handler are shown in the following format.
|
|
|
Non-operational state (STP state)
|
|
|
Operational state (STA state)
|
|
|
Non-existent cyclic handler
|
|
|
The ID of the cyclic handler is shown.
|
|
|
The current status of the cyclic handler is shown.
|
|
|
Non-operational state (STP state)
|
|
|
Operational state (STA state)
|
|
|
The activation cycle of the cyclic handler is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
|
|
|
The initial activation phase of the cyclic handler is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
|
|
|
The time left before the next activation of the cyclic handler is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
|
|
|
The start address of the cyclic handler is shown.
|
|
|
The extended information of the cyclic handler is shown.
|
|
|
The attributes of the cyclic handler (initial activation state and existence of saved activation phases) are shown in the following format.
Initial activation state Existence of saved activation phases
|
[Initial activation state of cyclic handler]
|
|
|
Operational state (STA state)
|
|
|
Non-operational state (STP state)
|
[Existence of saved activation phases]
|
|
|
There are saved activation phases.
|
|
|
There are no saved activation phases.
|