Everything

2.1 Overview

The resource information tool can be used to confirm the RI600V4 resource information (e.g. system information and memory area information) that changes dynamically as the program executes.
The operating procedures for the resource information tool are described below.
(1) Start CubeSuite+
Launch the CubeSuite+ from the [start] menu of Windows.
Remark See "CubeSuite+ Start" for details on "Start CubeSuite+".
(2) Open project
Open the project to debug.
Remark See "CubeSuite+ Start" for details on "Open project".
(3) Select debug tool
Select the type of debugging tool with which to debug the program (E1, E20 or Simulator).
Remark See "CubeSuite+ RX Debug" for details on "Select debug tool".
(4) Download programs
Download the program to debug.
Remark See "CubeSuite+ RX Debug" for details on "Download programs".
Remarks 1. When a program using the RI600V4 functionality is downloaded, this panel opens automatically.
2. The value will be indeterminate for the RI600V4 resource information shown when the RI600V4 system initialization is incomplete, because it will not be managed by the RI600V4.
(6) Execute/stop programs
Run the program to the location for which you wish to display the RI600V4 resource information.
Remark See "CubeSuite+ RX Debug" for details on "Execute/stop programs".
On the Realtime OS Resource Information panel tabs (e.g. [System] tab and [Memory Area] tab), check the current status of the RI600V4 resource information.