Everything

[Memory Area] tab

This tab displays the memory area information (e.g. Area Name and Top Address) of the RI600V4.
Figure A-3. [Memory Area] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
This area displays the memory area information (e.g. Area Name and Top Address) of the RI600V4.
This area consists of the following items.
Area Name
The name of the managed memory area is shown.
FIX_INTERRUPT_VECTOR
Area where the section for the fixed interrupt vector table is to be allocated.
INTERRUPT_VECTOR
Area where the section for the relocatable interrupt vector table is to be allocated.
SI
Area where the section for the system stack is to be allocated.
Top Address
The start address of the managed memory area is shown.
Size
The size of the managed memory area (in bytes) is shown.

[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Area Name, Top Address, Size
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
Top Address, Size
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Jump to Memory (Top Address)
Opens the Memory panel, and displays the contents of the managed memory area.
Reset Display Item
Resets the item displayed to initial state.