Everything

Realtime OS Resource Information panel

This panel displays the RI600V4 resource information (e.g. system information and memory area information) of the RI600V4.
Figure A-1. Realtime OS Resource Information Panel
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Tab selection area
Select a tab to switch the content displayed in the Information display area.
This panel has the following tabs:
(2) Information display area
This area displays the RI600V4 resource information (e.g. system information and memory area information) of the RI600V4.