Everything

[System] tab

This tab displays the system information (e.g. RTOS Name and Version) of the RI600V4.
Figure A-2. [System] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
This area displays the system information (e.g. RTOS Name and Version) of the RI600V4.
This area consists of the following items.
RTOS Name
"RI600V4" is shown.
Version
The version of the RI600V4 is shown.
System Time
The system time of the RI600V4 (in milliseconds) is shown.
Interrupt Nest
"--" is shown.
Dispatching
The system state of the RI600V4 is shown.
Disable
Dispatch disabled state
Enable
Dispatch enabled state
CPU Lock
The system state of the RI600V4 is shown.
Locked
CPU locked state
Unlocked
CPU unlocked state
System Stack Area
The start address, end address, and size (in bytes) of the system stack are shown in the following format.
Start address - End address (Size)
Current System SP
The current system stack pointer is shown.
Idle Routine
"--" is shown.
Number of Priority
The maximum priority of the task is shown.
Number of Task
The total number of tasks is shown.
Number of Semaphore
The total number of semaphores is shown.
Number of Eventflag
The total number of eventflags is shown.
Number of Data Queue
The total number of data queues is shown.
Number of Mailbox
The total number of mailboxes is shown.
Number of Mutex
The total number of mutexes is shown.
Number of Message Buffer
The total number of message buffers is shown.
Number of Fixed-Sized Memor Pool
The total number of fixed-sized memory pools is shown.
Number of Variable-Sized Memory Pool
The total number of variable-sized memory pools is shown.
Number of Cyclic Handler
The total number of cyclic handlers is shown.
Number of Alarm Handler
The total number of alarm handlers is shown.
Number of Interrupt Handler
"--" is shown.
Number of Initialize Routine
"--" is shown.
Number of Extended Service Call Routine
"--" is shown.

[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header column
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
RTOS Name, Version, System Time, Interrupt Nest, Dispatching, CPU Lock, System Stack Area, Current System SP, Idle Routine, Number of Priority, Number of Task, Number of Semaphore, Number of Eventflag, Number of Data Queue, Number of Mailbox, Number of Mutex, Number of Message Buffer, Number of Fixed-Sized Memory Pool, Number of Variable-Sized Memory Pool, Number of Cyclic Handler, Number of Alarm Handler, Number of Interrupt Handler, Number of Initialize Routine, Number of Extended Service Call Routine
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
System Time, System Stack Area, Current System SP, Idle Routine, Number of Priority, hing, CPU Lock, Stack Area, Current SP, Idle Routine, Number of Priority, Number of Task, Number of Semaphore, Number of Eventflag, Number of Data Queue, Number of Mailbox, Number of Mutex, Number of Message Buffer, Number of Fixed-Sized Memory Pool, Number of Variable-Sized Memory Pool, Number of Cyclic Handler, Number of Alarm Handler, Number of Interrupt Handler, Number of Initialize Routine, Number of Extended Service Call Routine
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer column
Jump to Memory (Current System SP)
Opens the Memory panel, and displays the contents of the Current System SP.
Reset Display Item
Resets the item displayed to initial state.