Everything

[Mailbox] tab

This tab displays the mailbox information (e.g. Mailbox Name and ID) of the RI600V4.
Figure A-14. [Mailbox] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
(a) First layer
This layer displays the mailbox information (e.g. Mailbox Name and ID) of the RI600V4.
This layer consists of the following items.
Mailbox Name
An icon indicating the current status of the mailbox and the name of the mailbox are shown in the following format.
Icon Name
There are waiting tasks.
There are waiting messages.
There are no waiting tasks/messages.
ID
The ID of the mailbox is shown.
Queue Status
The current status of the mailbox is shown.
Waiting Tasks
There are waiting tasks.
Waiting Messages
There are waiting messages.
Empty
There area no waiting tasks/messages.
Message Max Priority
The maximum priority of the message is shown.
If the message queuing method is TA_MFIFO, then "--" is shown.
Attribute
The attributes of the mailbox (task queuing method and message queuing method) are shown.
[Task queuing method]
TA_TFIFO
FIFO order
TA_TPRI
Task priority order
[Message queuing method]
TA_MFIFO
FIFO order
TA_MPRI
Message priority order

(b) Second layer
<1> Waiting task information
The waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the mailbox's wait queue.
See the [Task] tab for details about waiting task information.
Figure A-15. [Mailbox] Tab (Waiting Task Information)
<2> Waiting message information
The waiting message information (e.g. Message Address and Message Priority) only appears if there are messages queued in the mailbox's wait queue.
Figure A-16. [Mailbox] Tab (Waiting Message Information)
This area consists of the following items.
Message Address
The start address of the message is shown.
Message Priority
The priority of the message is shown.

[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Mailbox Name, ID, Queue Status, Message Max Priority, Attribute
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
ID, Message Max Priority
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Reset Display Item
Resets the item displayed to initial state.