Section specification
The section specification options are as follows.
-
-STARt
-FSymbol
-USER_OPT_BYTE
-OCDBG
-SECURITY_OPT_BYTE [V1.12 or later]
-SECURITY_ID
-FLASH_SECURITY_ID [V1.12 or later]
-AUTO_SECTION_LAYOUT
-SPLIT_SECTION [V1.12 or later]
-STRIDE_DSP_MEMORY_AREA [V1.12 or later]
-DEBUG_MONITOR
-RRM
-SELF
-SELFW
-OCDTR
-OCDTRW
-OCDHPI
-OCDHPIW
-STRIDE_SELF_AREA [V1.15.00 or later]
-STRIDE_OCDTR_AREA [V1.15.00 or later]
-STRIDE_OCDHPI_AREA [V1.15.00 or later]
-AVOID_SADDR_STACK [V1.15.00 or later]
-DSP_MEMORY_AREA [V1.12 or later]