Everything

 

-STRIDE_OCDTR_AREA [V1.15.00 or later]


This option allocates sections to split areas excluding the trace RAM area.

[Specification format]

-STRIDE_OCDTR_AREA

 

-

Interpretation when omitted

It is possible to allocate a section to the trace RAM area.

[Detailed description]

-

This option allocates sections to split areas excluding the trace RAM area.

[Example of use]

-

To allocate sections to split areas excluding the trace RAM area, describe as:

> rlink a.obj b.obj -device=dr5f10a6e.dvf -auto_section_layout -stride_ocdtr_ area

[Remark]

-

If the -form={object|relocate|library} or -strip option is specified, this option will be invalid.

-

If the -device option is not specified, this option will be invalid.