This option specifies the memory area for the OCD monitor.
The memory area for the OCD monitor is not allocated.
Specify the start address for the OCD monitor as address1 and the end address for the OCD monitor as address2. |
When the start address for the OCD monitor and the end address for the OCD monitor are omitted, the following is assumed to be specified. (For details on groups, see "Table 1.1 Group Notation".) |
Start address for OCD monitor: End address for on-chip ROM - 512 + 1
End address for OCD monitor: End address for on-chip ROM
Start address for OCD monitor: End address for on-chip ROM - 512 + 1
End address for OCD monitor: End address for on-chip ROM
[V1.10 or earlier] This option fills addresses 0x2, 0x3, and 0xCE to 0xD7 and the area from the OCD monitor start address to the OCD monitor end address with 0xFF. |
[V1.11 or later] This option fills addresses 0x2 and 0x3, the area conforming to device specifications, and the area from the OCD monitor start address to the OCD monitor end address with 0xFF. |
The area of addresses 0x2 and 0x3 which is also the vector table gives priority to the following specifications. |
When the memory area for the OCD monitor includes the location to allocate the user option bytes, the following specifications are given priority. |
When the memory area for the OCD monitor includes the location to allocate the control value for on-chip debugging, the following specifications are given priority. |
When the memory area for the OCD monitor includes the location to allocate the security ID value, the following specifications are given priority. |
If the -form={object|relocate|library} option or -strip option is specified, this option will be invalid. |