Everything

 

-DSP_MEMORY_AREA [V1.12 or later]


This option disables allocation of a section to the memory area shared with the FLEXIBLE APPLICATION ACCELERATOR (FAA).

[Specification format]

-dsp_memory_area

 

-

Interpretation when omitted

It is possible to allocate a section to the memory area shared with the FLEXIBLE APPLICATION ACCELERATOR (FAA).

[Detailed description]

-

This option disables allocation of a section to the memory area shared with the FLEXIBLE APPLICATION ACCELERATOR (FAA).

[Example of use]

-

To disable allocation of a section to the memory area shared with the FLEXIBLE APPLICATION ACCELERATOR (FAA), describe as:

>rlink a.obj b.obj -device=dr5f100pj.dvf -auto_section_layout -dsp_memory_area

[Remark]

-

If the -form={object|relocate|library} or -strip option is specified, this option will be invalid.

-

If the -device option is not specified, this option will be invalid.