Tangent
[Classification]
Mathematical library
[Syntax]
#include <math.h>
double  __far   tan(double x);
[Return value]
Returns the tangent of x.
If x is Not-a-Number or ±∞, tan returns a Not-a-Number (NaN) and sets macro EDOM to global variable errno.
If the solution is a denormal number, tan sets macro ERANGE to global variable errno.
[Description]
This function calculates the cosine of x.  Specify the angle in radian.