|
nearbyintl [V1.09 or later]
|
This function rounds the argument to an integer value in a floating-point format according to the rounding direction.
[Classification]
Mathematical library
[Syntax]
#include <math.h>
long double __far nearbyintl(long double x); (C99)
[Return value]
Returns a rounded value.
[Description]
This function rounds the argument to an integer value in a floating-point format according to the rounding direction.