|
copysign [V1.09 or later]
|
This function generates a value that has the absolute value of x and the sign of y.
[Classification]
Mathematical library
[Syntax]
#include <math.h>
double __far copysign(double x, double y); (C99)
[Return value]
Returns a value that has the absolute value of x and the sign of y.
[Description]
This function generates a value that has the absolute value of x and the sign of y.