Windows/panels/dialog boxes for debugging are listed below.
| 
 Controls the program execution. Various windows, panels and dialog boxes can be opened from this window.  | 
|
| 
 Selects a core (PE) to be debugged and displays the core status.  | 
|
| 
 Displays detailed information on the debug tool currently selected in the Project Tree panel, and enables the settings of the tool to be changed.  | 
|
| 
 Displays the results of memory value disassemble and is used to execute line assemble and instruction level debug.  | 
|
| 
 Displays the contents of CPU registers, and modifies register values.  | 
|
| 
 Displays detailed information on set events, switches the events between enabled and disabled, or deletes them.  | 
|
| 
 Displays messages output from the build tool/debug tool/plug-ins, or the results of batch searches carried out using the Find and Replace dialog box.  | 
|
| 
 Sets the contexts on the debug target which details are displayed.  | 
|
| 
 Selects files to be downloaded and sets the download conditions.  | 
|
| 
 Specifies the number of view columns of memory values on the Memory panel.  | 
|
| 
 Specifies an offset value for the address display on the Memory panel.  | 
|
| 
 Sets the address range to print the contents of the Disassemble panel.  | 
|
| 
 Displays and modifies the detailed information on an execution-related event.  | 
|
| 
 Displays and modifies the detailed information on an access-related event.  | 
|
| 
 Displays and modifies the detailed information on the point trace event.  | 
|
| 
 Detailed Settings of Timer Measurement dialog box [Full-spec emulator][E1][E20]  | 
 Displays and modifies the detailed information on the timer event.  | 
| 
 Detailed Settings of Performance Measurement dialog box [Full-spec emulator][E1][E20]  | 
 Displays and modifies the detailed information on the Performance Measurement event.  | 
| 
 Sets the scroll range for the Memory panel/Disassemble panel.  | 
|
| 
 Saves the settings and other data displayed in the respective windows/panels/dialog boxes or saves upload data.  | 
|
| 
 Displays the functions that access variables in the form of an orthogonal table.  | 
|
| 
 Checks whether exclusive control is correctly performed for a certain variable and makes the settings required for checking.  | 
|
| 
 This panel is central to the functionality of the solution for pseudo-error debugging.  | 
|
| 
 Select Pseudo-Error dialog box [Full-spec emulator][E1][E20]  | 
 Selects ECM pseudo-errors displayed in the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20].  | 
| 
 Sets the breakpoints that are to be registered to the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20].  | 
|
| 
 Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20]  | 
 This panel is central to the functionality of the solution for debugging of CAN bus reception.  | 
| 
 RS-CAN Module Setting dialog box [Full-spec emulator][E1][E20]  | 
|
| 
 Receive Channel Setting dialog box [Full-spec emulator][E1][E20]  | 
|
| 
 Transmit Channel Setting dialog box [Full-spec emulator][E1][E20]  | 
|
| 
 Transmit Frame Setting dialog box [Full-spec emulator][E1][E20]  | 
|
| 
 This panel is central to the functionality of the solution for measurement of CAN bus reception processing times.  | 
|
| 
 This dialog box is used to set conditions for measurement in the Measuring CAN Bus Reception Processing Times panel [E2].  |