This option automatically allocates sections.
Sections are not automatically allocated.
After the section specified by the -start option and the absolute address sections have been allocated, the remaining sections are automatically allocated based on the information of the device file. |
With the -cpu option specified, -AUTO_SECTION_LAYOUT automatically allocates sections to an address in the range from address1 to address2 designated by the -cpu option and within the memory space defined in the device file designated by the -device option. |
If the -form={object|relocate|library} option or -strip option is specified, this option will be invalid. |