This option disables allocation of a section to the memory area shared with the FLEXIBLE APPLICATION ACCELERATOR (FAA).
It is possible to allocate a section to the memory area shared with the FLEXIBLE APPLICATION ACCELERATOR (FAA).
This option disables allocation of a section to the memory area shared with the FLEXIBLE APPLICATION ACCELERATOR (FAA). |
To disable allocation of a section to the memory area shared with the FLEXIBLE APPLICATION ACCELERATOR (FAA), describe as: |