This option outputs a warning message when a section is allocated to the trace RAM and self RAM areas.
The trace RAM and self RAM areas are not checked.
This option outputs a warning message when a section is allocated to the trace RAM and self RAM areas. |
To output a warning message when a section is allocated to the trace RAM and self RAM areas, describe as: |
If the -form={object|relocate|library} option or -strip option is specified, this option will be invalid. |