This option disables allocation of a section to the hot plug-in RAM, trace RAM, and self RAM areas.
It is possible to allocate a section to the hot plug-in RAM, trace RAM, and self RAM areas.
This option disables allocation of a section to the hot plug-in RAM, trace RAM, and self RAM areas. |
To disable allocation of a section to the hot plug-in RAM, trace RAM, and self RAM areas, describe as: |
If the -form={object|relocate|library} option or -strip option is specified, this option will be invalid. |