本API関数では,データ(引数adrで指定されたスレーブ・アドレス)をスレーブ・デバイスにSCIマスタ送信したのち,1バイト単位のSCIマスタ受信を引数rx_numで指定された回数だけ繰り返し行い,引数rx_bufで指定されたバッファに格納します。 |
本API関数では,SCIマスタ受信の開始処理として,内部的にR_SCIn_IIC_StartConditionの呼び出しを行っています。 |
SCIマスタ受信を行う際には,本API関数の呼び出し以前にR_SCIn_Startを呼び出す必要があります。 |
#include "r_cg_macrodriver.h" void R_SCIn_IIC_Master_Receive ( uint8_t adr, uint8_t * const rx_buf, uint16_t rx_num ); |