-preinclude


< Compile Options / Source Options >

[Format]

-preinclude=<file name>[,...]

[Description]

-

This option includes the specified file contents at the head of the compiling unit. Multiple file names can be specified by separating them with a comma (,).

-

If there is more than one folder specified by the preinclude option, search is performed in turn starting from the leftmost folder.

[Remarks]

-

If this option is specified for more than one time, all specified files will be included.