-ignore_files_misra [Professional Edition only]


< Compile Options / Source Options >

[Format]

-ignore_files_misra=<filename>[,<filename>,...]

[Description]

-

This option selects source files that will not be checked against the MISRA-C:2004 rules or MISRA-C:2012 rules.

[Remarks]

-

If the option is specified more than once in the command line, all specifications are valid.

-

This option is ignored when the misra2004 or misra2012 option has not been specified.

-

<filename> is ignored when the specified file is not to be compiled.