-undefine


< Compile Options / Source Options >

[Format]

-undefine=<sub>[,...]
          <sub>: <macro name>

[Description]

-

This option invalidates the predefined macro of <macro name>.

-

Multiple macro names can be specified by separating them with a comma (,).

[Remarks]

-

Refer to the Macro Names section, in the COMPILER LANGUAGE SPECIFICATIONS chapter, for specifiable predefined macros of the compiler.

-

If this option is specified for more than one time, all specified macro names will be undefined.