r_uartn_callback_sendend


Performs processing in response to the UART transmission end interrupt INTSTn.

Remark

This API function is called as the callback routine of interrupt process r_uartn_interrupt_send corresponding to the UART transmission end interrupt INTSTn (performed when number of transmission data specified by R_UARTn_Send argument tx_num has been completed).

[Syntax]

static  void    r_uartn_callback_sendend ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.