r_csimn_interrupt


Performs processing in response to the CSI communication end interrupt INTCSImn.

Remark

This API function is called as the interrupt process corresponding to the CSI communication end interrupt INTCSImn.

[Syntax]

__interrupt static  void    r_csimn_interrupt ( void );

Remark

m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.