Performs processing in response to the simple IIC communication end interrupt INTIICmn.
| 
Remark | This API function is called as the interrupt process corresponding to the simple IIC communication end interrupt INTIICmn. | 
[Syntax]
| __interrupt static  void    r_iicmn_interrupt ( void ); | 
| 
Remark | m is the unit number, and n is the channel number. | 
[Argument(s)]
None.
[Return value]
None.