R_IICmn_Create


Performs initialization necessary to perform the simplified IIC communication.

Remark

This API function is used as an internal function of R_SAUm_Create.
For this reason, there is normally no need to call it from a user program.

[Syntax]

void    R_IICmn_Create ( void );

Remark

m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.