Starts CSI data transmission.
| 
Remarks 1. | This API function repeats the byte-level CSI transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num. | 
| 
Remarks 2. | When performing a CSI transmission, R_CSImn_Start must be called before this API function is called. | 
[Syntax]
| #include    "r_cg_macrodriver.h" MD_STATUS   R_CSImn_Send ( uint8_t * const tx_buf, uint16_t tx_num ); | 
| 
Remark | m is the unit number, and n is the channel number. | 
[Argument(s)]
|  |  |  | 
|  | uint8_t   * const tx_buf; | 
Pointer to a buffer storing the transmission data | 
|  | uint16_t  tx_num; | 
Total amount of data to send | 
[Return value]
|  |  | 
| 
MD_OK | 
Normal completion | 
| 
MD_ARGERROR | 
Invalid argument specification |