The following can be specified for vector:
For details of the function, see the Relevant Device's Architecture User's Manual of each device. |
If an absolute expression having a value falling outside the range of 0 to 31 is specified as vector, the assembler outputs the following message, continuing assembling using the lower 5 bitsNote of the specified value. |
The trap machine instruction takes an immediate value in the range of 0 to 31 (0x0 to 0x1F) as an operand. |