double fmod(double x, double y);
Returns a floating-point value that is the remainder resulting from dividing x by y.
If x is + or y is zero, fmod returns a Not a Nuber(NaN) and sets macro ERANGE to global variable errno.
This function calculates a floating-point value that is the remainder resulting from dividing x by y. In other words, it calculates the value "x - i * y" for the maximum integer i that has a sign the same as x and is less than y, if y is not zero.